5/13/2019 5:20 AM | |
Joined: 12/18/2014 Last visit: 8/31/2024 Posts: 33656 Rating: (4183)
|
The Aq value in the parameter table below the mathematical block is only updated in simulation mode. See attached video. AttachmentOnline Test.zip (522 Downloads) |
This contribution was helpful to3 thankful Users |
5/13/2019 10:19 AM | |
Posts: 4 Rating: (0) |
Thank you, very much for all your help. So will my program still work - allowing temperature adjustment on the threshold trigger blocks even though the parameter tables below the function blocks are not populated/updated with new information as I change values with the up/down counter? Is it just the way the information is displayed on Logo!Soft? Thanks for pointing out the problem casued by the ESC key, I have changed the cursor keys to inputs on the program and LWE (as I have run out of available function keys) Here is a copy of the program in case it helps: [snip] Very much appreciated again. Robbie Crewe AttachmentWhite Cross BEMS.zip (646 Downloads) |
Last edited by: Jen_Moderator at: 05/13/2019 11:38:24Removed link and added file as an attachment. |
|
5/13/2019 10:37 AM | |
Joined: 12/18/2014 Last visit: 8/31/2024 Posts: 33656 Rating: (4183)
|
See attached screen video of your program in online test.
AttachmentOnline Test.zip (537 Downloads) |
5/13/2019 10:49 AM | |
Joined: 12/18/2014 Last visit: 8/31/2024 Posts: 33656 Rating: (4183)
|
Hello Robbie Crewe, you're welcome... |
5/13/2019 11:38 AM | |
Posts: 4 Rating: (0) |
Thank you, I will set that up for each heater. |
Follow us on