10/12/2019 1:49 PM | |
Joined: 9/20/2018 Last visit: 1/2/2024 Posts: 42 Rating: (4) |
Hii, I'm also facing same issue. I'm having 15 slave and 15 task. Out of 15 ,10 are assigned in S7HMODM3 and remaining are assigned in EXSQ_MOD block. For 10 task i'm getting no error. But from 11 to 15 i'm getting error (Error NO-5). As result I'm not able to get reading from slave devices which are assigned in EXSQ_MOD block. I also cross checked with MODSCAN software all Modbus Slave devices are correctly configured and connected. I also connected QEXT_LIN to MST_LINk of EXSQ_MOD block. CHAIN is ON. MST_CONN is 1. Also both block are in same RUN SEQUENCES. Please revert. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/14/2019 11:27:25New subject after splitting |
|
Follow us on