12/9/2019 3:10 AM | |
Posts: 5 Rating: (2) |
Hi all, Every time I attempt to download a LWE project to LOGO! I receive this message (screenshots in attachments). Same error if a try to upload the project. I could not find this error in any manual of LWE, LSC and so on. A feel facts: 1- SD card if formatted in FAT32 (not fast format) as per system manual 2- In LWE the function "Deploy to SD card" works but in web server I have the 404 error 3- Everything is allowed regading access control in LSC 4- I can access webserver without check "to customized site" 5- Diagnostic function on LSC can distinguish if the SD card is inserted or not Thanks in advance! Attachmentlwe.zip (496 Downloads) |
12/9/2019 4:33 PM | |
Joined: 12/18/2014 Last visit: 10/6/2024 Posts: 33882 Rating: (4215)
|
Hello Gumiero, thanks for the feedback. Maybe it helps other users who have the same or a similar problem. |
Follow us on