4/10/2020 1:59 PM | |
Posts: 5 Rating: (0) |
Hello, I have a problem with a VBScript. I´m trying to send some values to a Database using VBScript, but when I select the Tag to be read and inserted into the database it gives an error, in this case: " HmiRuntime.Tags("Start_HMI").Read does not produce a value." I have tried also with integer and float Tags but the same result. I can simulate without problems though. I attach a screenshot with the problem. If anybody have any idea please tell me. I´m stuck here. I´m using TIA Portal V16 Profesional and WinCC Profesional V16 Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/14/2020 08:59:33New subject after splitting |
|
4/13/2020 5:51 AM | |
Joined: 3/2/2015 Last visit: 7/19/2024 Posts: 11 Rating: (0) |
Hi, For Tia WnCC avanced use SmartTags("TagName"). May be HmiRuntime.Tags structure actually for Professional version. |
4/28/2020 12:58 PM | |
Joined: 8/3/2009 Last visit: 7/29/2024 Posts: 13392 Rating: (1700)
|
Hello Jorge you should be able to use this example also for WinCC Professional: https://support.industry.siemens.com/cs/ww/en/view/61883659 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on