6/17/2020 4:14 PM | |
Posts: 6 Rating: (0) |
Hello I am working on example from this page: I opened the project, changed the device to my actual one, set the credidential as they should be and I always get an error 8602 which means Error when calling TCON when I modify the input enable to true. Can someone point me on the right path. I have years of experiance with SQL, but this thing is killing me :) Tnx. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/18/2020 08:04:14New subject after splitting. Optimized link. Last edited by: CS Moderator at: 11/16/2020 08:31:56Subject optimized |
|
This contribution was helpful to1 thankful Users |
Follow us on