8/7/2020 5:06 AM | |
Posts: 1 Rating:
|
Have a good day EveryBody. Diag Buffer Nr Time Date Event 126 06:57:45.739 06.08.20 Technological alarm uw3b: Alarm 20005 : Device type:1, log. address:364 faulted. (Bit:0, encoder number:0, reason: 0x1h) 127 06:57:45.739 06.08.20 Technological alarm uw3a: Alarm 20005 : Device type:1, log. address:344 faulted. (Bit:0, encoder number:0, reason: 0x1h) 128 06:57:45.271 06.08.20 Technological alarm uw1b: Alarm 20005 : Device type:1, log. address:324 faulted. (Bit:0, encoder number:0, reason: 0x1h) 129 0 6:57:45.067 06.08.20 Technological alarm uw1a: Alarm 20005 : Device type:1, log. address:304 faulted. (Bit:0, encoder number:0, reason: 0x1h) 130 06:56:54.508 06.08.20 Technological alarm uw2b: Alarm 20005 : Device type:1, log. address:650 faulted. (Bit:0, encoder number:0, reason: 0x1h) 131 06:56:54.499 06.08.20 Technological alarm uw2a: Alarm 20005 : Device type:1, log. address:730 faulted. (Bit:0, encoder number:0, reason: 0x1h) 66 07:08:46.883 06.08.20 Technological alarm uw4b: Alarm 20005 : Device type:1, log. address:486 faulted. (Bit:0, encoder number:0, reason: 0xC000h) 67 07:08:46.883 06.08.20 Technological alarm uw4a: Alarm 20005 : Device type:1, log. address:630 faulted. (Bit:0, encoder number:0, reason: 0xC001h) 68 07:08:46.874 06.08.20 Technological alarm uw4b: Alarm 20005 : Device type:1, log. address:486 faulted. (Bit:0, encoder number:0, reason: 0x8000h) 69 07:08:46.874 06.08.20 Technological alarm 70 07:08:46.880 06.08.20 PROFIBUS DP 1: Station failure, node 4 71 07:08:46.862 06.08.20 Technological alarm PLS I am needing orientation to resolve this case.------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/07/2020 06:57:12New subject after splitting |
|
8/7/2020 6:26 AM | |
Joined: 5/12/2006 Last visit: 7/25/2024 Posts: 22324 Rating:
|
Hi, please post the complete diagnostic buffer. And what you mean with "Go automatic to run"? Christoph |
7/17/2022 6:15 AM | |
Joined: 9/1/2015 Last visit: 6/18/2024 Posts: 15 Rating:
|
Did you solve this problem? I had the same problem! |
7/18/2022 5:47 AM | |
Joined: 5/12/2006 Last visit: 7/25/2024 Posts: 22324 Rating:
|
describe your prolem |
Follow us on