3/9/2021 5:46 AM | |
Posts: 198 Rating: (60) |
Hello, If you are unsure about an MLFB number and its exact usage or description, try to use the 'product search' option in the Industry Mall and refer to relevant datasheets (if available) In this case, I have some information for you. 6ES7653-2BA00-0XB5 - SIMATIC PCS 7, software, Runtime License AS (PO 100), Floating license for 1 user R-SW, without SW, without documentation License Key on USB stick, Class A, Reference HW: PCS 7 IPC Bundle, PCS 7 Box Bundle ******************************* Content: 1x USB As of PCS7 V7.0, Process objects (PO) requiring licenses include objects that are subject to operator control and monitoring and can generate messages. These objects have the block attribute "S7_m_c" and require the "PCS 7 - Runtime License AS" license with the "AS RT PO" license key. Hence based on my understanding, it will not be relevant to a PCS7 V8.1 setup where ASRTPO licenses can be used separately for the process objects. Kindly refer the Licenses configuration manual for better information and explanation. Hope this helps! :) |
3/9/2021 11:36 AM | |
Posts: 198 Rating: (60) |
Hello, As mentioned in my above explanation, it will not be possible to use for your requirement. |
This contribution was helpful to1 thankful Users |
Follow us on