5/13/2021 7:25 AM | |
Joined: 3/30/2020 Last visit: 10/19/2024 Posts: 4884 Rating: (996) |
Hello. What you described as a symptom sounds like the type problem you will get from a missing terminating resistor. There is such a thing as too short device-to-device cable length. This depends on the baud rate. You can use the Profibus specification. Not to say that this is the cause. A nice application example which I have used on the V20 drive: The example explains everything. ~ |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on