7/9/2021 8:08 AM | |
Joined: 6/10/2015 Last visit: 9/10/2024 Posts: 468 Rating: (95) |
Hi all, on Win 10 some package does not get installed. Attached is a log. I already tried to repair, but the same message appears. 17:48:49 |WARNING InstallResultSetupPackage::ReadResult(): - LocalLogging - Setup Package Message: Type(Error); Severity(AfterInstall); Text(The EditionMain WinCCUnified isn't installed or doesn't have the required version.| found version: | allowed version: min 3.0.0.0 | 17:48:49 |ERROR AdsWorkerSetupPackage::OnWorkerCompleted(): - SetupPackage setup failed due to unknown error Indicated FAQ does not help much. https://support.industry.siemens.com/cs/ww/en/ps/14667/faq Did anyone have experienced this, before? Can it be due to the fact that, existing v15.1 and 16 on my pc, I uninstall 16, and when installing 17 I first install step 7 and then TiA 17? Thank you AttachmentSIA_STEP7_S7FPLUS_WINCC_ADV_V17@21-07-08_17-10-32_AFTERREBOOT_summary.txt (738 Downloads) |
B. Edulis |
|
This contribution was helpful to3 thankful Users |
7/9/2021 8:33 AM | |
Joined: 6/10/2015 Last visit: 9/10/2024 Posts: 468 Rating: (95) |
Here it is. Folder is C:\ProgramData\Siemens\Automation\Logfiles\Setup I cut the first part in order to be less than 3MB in space. On summary, error was around time17:48:xy
AttachmentSIA_STEP7_S7FPLUS_WINCC_ADV_V17@21-07-08_17-10-32_AFTERREBOOT.txt (479 Downloads) |
B. Edulis |
|
7/9/2021 8:57 AM | |
Joined: 6/10/2015 Last visit: 9/10/2024 Posts: 468 Rating: (95) |
ADS_ERROR COUNT changes at line 678 and 701 of the log file At the end is 2
this is the RESULT.LOG [Messages] Count=1 Message1=The EditionMain WinCCUnified isn't installed or doesn't have the required version.| found version: | allowed version: min 3.0.0.0 | Type1=1 Critical1=2 [Results] ADS_SIARESULT_REBOOT=0 ADS_SIARESULT_RESULT=1 ADS_SIARESULT_ERRORS=2 ADS_SIARESULT_WARNINGS=0 AttachmentLocalLogging_WinCCUnified_Setup.txt (376 Downloads) |
Last edited by: BoletusEdulis at: 07/09/2021 08:59:45B. Edulis |
|
7/9/2021 9:08 AM | |
Joined: 6/10/2015 Last visit: 9/10/2024 Posts: 468 Rating: (95) |
here it is
AttachmentLocalLogging_WinCCUnified_Setup_RESULT.txt (381 Downloads) |
B. Edulis |
|
Follow us on