9/16/2021 10:25 AM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
Your driver choice S7 over TCP is okay, the addressing is like a s7-200. Therefore it may be, you have to use I0.0 for I1 up to I0.7 for I8, I1.0 for I9 up to I1.7 for I16 and so on. The same numbering is to use for Qx, Mx and Vx. Normally there is an online help also for the driver, which operands can be used. The addressing of analog signals can be done with AIWx (AI1 may be AIW0), AQWx (AQ1 may be AQW0), VWx (VW0=VW0 for 16 bit integer e.g. arithmetic values), VDx (VD0=VD0 for 32 bit integer e.g. counter values). These are the addressing modes in the past for older HMI displays. See also following link from beijers, you can change the language. Regards, Scorp |
Last edited by: Scorp at: 09/16/2021 11:23:50 |
|
9/16/2021 12:32 PM | |
Joined: 12/18/2014 Last visit: 8/30/2024 Posts: 33647 Rating: (4182)
|
Which LOGO!Soft version use you? |
9/16/2021 1:10 PM | |
Joined: 2/11/2013 Last visit: 10/26/2023 Posts: 21 Rating: (0) |
I use version 8.3. Also, how can I know which hardware type I have. My LOGO is 6ED1052-1MD08-0BA1 . Inside online help of LOGO soft 8.3, it says: If you have version 0BA8 do this..... If you have version 0BA7 do this..... If you have version 8.FS4 do this..... I am confused! FS what is? Firmware version? Many thanks for your support! |
Last edited by: b1naryc0deexe at: 09/16/2021 13:10:50 |
|
9/16/2021 1:23 PM | |
Joined: 12/18/2014 Last visit: 8/30/2024 Posts: 33647 Rating: (4182)
|
Your LOGO! is the current LOGO!8.3. In the device selection you have to select the LOGO!8.3. In you want to communicate with S7 protocol then have you to allow the S7 access. File > Properties > Offline settings > General > Ethernet connections In the same section you can make a server connection. Right click on the Ethernet Connection, then "Add server connection", then "S7 connection. Then is created Connection1. Double click on it. |
9/16/2021 1:35 PM | |
Joined: 2/11/2013 Last visit: 10/26/2023 Posts: 21 Rating: (0) |
Thanks! When you say that "my LOGO is current 8.3", which hardware type is? 0BA8? 0BA7? something else? At the following table, where shall I see for VM mapping? 0BA8 or 0BA7? |
Follow us on