5/18/2022 2:14 PM | |
Joined: 9/27/2021 Last visit: 5/19/2022 Posts: 2 Rating: (0) |
Hi All, Do anyone have any idea what's going on ? I bought this device, I hope it might help. It is enough right for only 4 pin to connect to the device ? (I'm using all except 5V pin) I have message bergmanu for this matter but it seems some trouble occur so i can't reply his message |
5/18/2022 5:03 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, which FS does your IOT2050 Advanced have? You can check how to connect the cable in this thread, third post. Hope that helps. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
5/19/2022 7:35 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, the FS:04 does not have an OS pre-installed. You need to flash the Example Image V1.2.2 to an SD card. Instructions see here. Unfortunately there is no Industrial OS available at the moment for FS:04. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
Follow us on