10/26/2022 1:14 PM | |
Joined: 9/6/2014 Last visit: 6/23/2024 Posts: 209 Rating:
|
hi guy Do you did general reset according to siemens manual? If yes , so maybe your ccu box damaged !!! best regards |
10/27/2022 3:41 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello M. Shafay, I guess you are talking about 810D system. I suggest you to follow below steps. 1. With RS232 & WinPCIN software always take backup of NC, PLC & store it on external media. 2. Please delete old/not required frequently part program, subprograms especially which are of bigger size. 3. When you want to store NC, PLC arc back up on NC card, please export old back up on external media & store it with all details like date, size, reason of back up etc. etc. This is good practice which will help you in future to identify the details of back up. 4. By regularly following step 3 & 4 user can free memory size/loading of NC card which will help user to run system with optimum capacity of NC area. 5. On machine/system itself, you can delete part programs, sub-programs of bigger size which will free NC memory area. You may delete those files, even after taking these files back up on external storage media. Hope this helps. |
This contribution was helpful to
1 thankful Users |
Follow us on