2/1/2023 4:31 AM | |
Joined: 5/12/2006 Last visit: 10/14/2024 Posts: 22411 Rating: (3017)
|
if you use 1504D TF no additional CU320-2 is need |
This contribution was helpful to1 thankful Users |
2/1/2023 11:05 AM | |
Joined: 12/20/2012 Last visit: 8/4/2024 Posts: 57 Rating: (0) |
Hi, Which model Servo Driver is integrated(independent control) control and no need to CU320-2 PN? such as S120 Thanks |
2/1/2023 11:08 AM | |
Joined: 5/12/2006 Last visit: 10/14/2024 Posts: 22411 Rating: (3017)
|
1504D have a integrated S120 based drive controller |
2/1/2023 12:51 PM | |
Joined: 12/20/2012 Last visit: 8/4/2024 Posts: 57 Rating: (0) |
Thanks, Solved. V90 driver's are integreted control but S120 is modular. |
Follow us on