2/26/2023 8:38 PM | |
Joined: 11/2/2021 Last visit: 4/15/2023 Posts: 3 Rating: (0) |
Hola, Realizó todo el proceso de la configuración de un iot2040 conforme a lo indica la guía. Tengo un inconveniente que suele ocurrir muy seguido, cuando estoy realizando conexiones en NODE-RED de un momento a otro se me desconecta el software y ya no puedo ingresar al NODE-RED con la dirección 192.168.200.1:1880, sin embargo en PUTTY puedo conectarme al IOT2040 hacer ping www.google.com y tengo conexion. ¿Cómo puedo solucionar eso rápidamente? Gracias ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/27/2023 11:04:28New subject after splitting |
|
2/28/2023 2:40 AM | |
Joined: 11/2/2021 Last visit: 4/15/2023 Posts: 3 Rating: (0) |
hi, attached as requested, Thanks Attachmentiot2040.txt (751 Downloads) |
3/1/2023 11:39 AM | |
Joined: 4/28/2015 Last visit: 11/12/2024 Posts: 3345 Rating: (379)
|
Hi, I think the problem is the version of the S7 node. Please see here. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
3/2/2023 12:04 AM | |
Joined: 11/2/2021 Last visit: 4/15/2023 Posts: 3 Rating: (0) |
Dear, I executed the commands to install the S7 and Ubidots nodes in the Node-red of my IOT 2040. When finishing the installation of each node, I got the errors and warnings that are in the attached document. I would like to know if these errors and warnings will affect the future operation of my IOT applications, PLC S7-1200 and UBIDOTS. Thanks for your timely help.
Attachmentinstall nodes s7 and ubidots.txt (872 Downloads) |
Follow us on