3/9/2023 7:30 AM | |
Joined: 9/23/2005 Last visit: 8/6/2024 Posts: 4659 Rating: (718) |
Profidrive is a specification of Profibus/Profinet telegrams and some other things. You should start from here. |
Regards, |
|
This contribution was helpful to1 thankful Users |
3/9/2023 7:46 AM | |
Joined: 1/21/2013 Last visit: 8/4/2024 Posts: 3044 Rating: (479)
|
Hi KevinNfoDrives, In chapter 3.9 of the 'SINAMICS S120/S150' list manual you will find some details about the standard PROFIdrive telegrams and the Siemens telegrams. Further details can be found on the PROFIBUS and PROFINET International (PI) website, where as a member you have access to extensive information. To see how a PROFIdrive-enabled drive is used in conjunction with S7-1200 technology objects, take a look at 'SINAMICS V: Position Control with SIMATIC S7-1200 TO and SINAMICS V90 PN (S mode)'. Kind regards |
3/14/2023 10:39 AM | |
Joined: 1/21/2013 Last visit: 8/4/2024 Posts: 3044 Rating: (479)
|
Hi KevinNfoDrives, PROFIdrive is an application profile for PROFINET and PROFIBUS. Basically, it describes the exchanged data and was created for better interoperability between different manufacturers. Since PROFIdrive almost defines the data, only the data types used in the PLC depend on PROFIdrive. Therefore, you would not see much of PROFIdrive in your PLC program other than the "PD_TELx" data types. In TIA Portal, the Motion Control Technology Objects are for motion control according to the PLCopen motion standard. The interface to the hardware is mostly done via PROFIdrive, except for the analog interface. More information about PROFIdrive is available from PROFIBUS & PROFINET International (PI):
Kind regards |
Follow us on