4/6/2023 5:36 AM | |
Joined: 1/21/2013 Last visit: 7/15/2024 Posts: 2987 Rating: (470) |
Hi dogukanbayir2, Your STL code contains the EXCLUSIVE OR logic operation. This cannot be represented in ladder logic. Therefore, you can't change the affected network to LAD. However, you can convert it to FBD. Switching the programming language to FBD first and then to LAD should result in a block that represents LAD where possible and FBD for the other networks. Kind regards |
This contribution was helpful to1 thankful Users |
4/6/2023 8:13 AM | |
Joined: 9/23/2005 Last visit: 7/15/2024 Posts: 4621 Rating: (712)
|
The link you provided shows opposite. Look at the relay circuit diagram next to the STL code. The LAD language from Boolean logic point of view is complete. I.e. it can express any combinatorial logic function. |
Last edited by: jacek d at: 04/06/2023 08:16:31Regards, |
|
Follow us on