4/13/2023 9:15 PM | |
Joined: 7/15/2022 Last visit: 9/7/2024 Posts: 8 Rating: (0) |
hello, I have a problem with send p2p and receive p2p, two devices are connected, if both work, then there are no problems, but if one is disabled, the values of the first one will write to both addresses. Using CB1241 for RS485 ------------------------------------------------------------------------------------------ |
Last edited by: Sarvarjon at: 04/13/2023 21:15:55Last edited by: Jen_Moderator at: 04/14/2023 06:46:16New subject after splitting |
|
4/15/2023 11:29 AM | |
Joined: 7/15/2022 Last visit: 9/7/2024 Posts: 8 Rating: (0) |
here is the screenshot |
4/16/2023 12:47 PM | |
Joined: 7/15/2022 Last visit: 9/7/2024 Posts: 8 Rating: (0) |
Ok thanks |
Follow us on