4/25/2023 4:39 AM | |
Joined: 11/5/2020 Last visit: 4/28/2023 Posts: 5 Rating:
|
Hello Any one have a download link Starter version 5.4.0.1 . Thanks |
4/25/2023 4:50 AM | |
Joined: 12/18/2014 Last visit: 7/24/2024 Posts: 33408 Rating:
|
There is no legal download from Siemens web sites. |
4/25/2023 4:56 AM | |
Joined: 1/21/2013 Last visit: 7/24/2024 Posts: 3012 Rating:
|
Hi shshakil, The following versions are currently available on the SINAMICS STARTER download page: V5.4 SP2 HF1 (V5.4.2.1) and V5.4 HF2 (V5.4.0.2). If you really need another version, you can try to get it by submitting a support request. Kind regards |
4/25/2023 8:51 AM | |
Joined: 1/21/2013 Last visit: 7/24/2024 Posts: 3012 Rating:
|
Hi shshakil, Unfortunately, using a different version of STARTER will not help you. You will get this message for a corrupted project. Corrupted project can happen even if you move the project to another folder, that's why you should always work with an archive. So if you are in a situation where you have an archived version, please try this. Otherwise, you will need to repair your project with the help of technical support, which may extend the possibilities of free support. However, in the case of STARTER, you can also upload almost everything from the device into a new project. Kind regards |
This contribution was helpful to
1 thankful Users |
Follow us on