4/8/2019 3:54 PM | |
Joined: 5/3/2017 Last visit: 2/6/2025 Posts: 673 Rating:
|
Hello AdamDPS, you can use the block StruDiIn to separating a binary process value into a variable of the BOOL data type and signal status. So you can connect the SEL input. Note:
There you can connect a input without signal status with an process value with signal status. With regards |
4/8/2019 4:24 PM | |
Joined: 9/9/2015 Last visit: 1/10/2025 Posts: 728 Rating:
|
Dear AdamDPS, I hope i understand your question correctly. You mentioned SEL block doesnt carry structure in the output. Are you using the SEL block in APL library named SelDiIn(sth like this)? There are all able to carry signal status. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on