Industry Online Support
Technical Forum
2/22/2017 9:41 PM | |
Posts: 1 Rating: (0) |
Hello I am using a cpu 315 2PN / DP and an DO 6ES7322-1BL00-0AA0 I need a frequency in the DO of 300 - 400 Hz, is this possible? |
2/23/2017 8:21 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1052) |
hi gomesaspitante,
The switching fequency is max. 100Hz. you can read this in the technical data of the Module hope this helps, regards |
FCK WAR! |
|
Follow us on