7/27/2023 12:02 PM | |
Joined: 2/1/2022 Last visit: 10/31/2023 Posts: 19 Rating: (3) |
Thread Necroing this so I can get help also. I am at the same point as the other user was, years ago. I can read the PAC4200, but slaves return the same value as the PAC4200. Yes, I am using port 17002. [attachment id="5742" /] [attachment id="5743" /] The PAC1020 should be address 126 on port 17002. But this returns same numbers as the PAC4200. I can access through PowerConfig no problem and it returns correct values.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/28/2023 07:57:00New subject after splitting. Quote inserted. |
|
Follow us on