8/1/2023 12:41 PM | |
Joined: 9/27/2006 Last visit: 7/20/2024 Posts: 12270 Rating: (2676) |
Hello; Maybe the following sceenshot can explain your problem? https://support.industry.siemens.com/cs/ca/en/view/58523240 Others on the forum have reported that eb¸ven if you manage to install icrowin on Windows 10 (64 bit), communication with the PLC is not possible, the PC/PPI Adapter drivers do not install properly. There are various threads here that discuss potential installation procedures of MicroWin v4.SP9 on Windows 10, such as this one; they mostly involve modifying registry entries: But the concensus remains that the simplest way would be to have a VM with Windows 7 64-bit, which will allow you to install the PC/PPI drivers, outside ow Windows 10. Hope this helps, |
Last edited by: dchartier at: 08/01/2023 12:42:34 |
|
Follow us on