9/26/2023 1:33 PM | |
Joined: 8/4/2014 Last visit: 1/29/2024 Posts: 23 Rating: (1) |
Dear TechTeam, I'm replying to this old topic with similar question. I have two drive configurations that I want to use with monitioring of SLS and SOS: 1) Configuration with encoder:
Question 1: Can you please check if Leine-Linde FSI 862 encoder is suitable to be used as single encoder with SMC30 for SLS and SOS monitoring or it must be used in 2-encoder configruation? [snip] Thank you! Best regards, Almen ------------------------------------------------------------------------------------------ |
Last edited by: Almen123 at: 09/26/2023 15:16:14Last edited by: Jen_Moderator at: 09/27/2023 07:31:07New subject after splitting. Division of question into separate topic. |
|
9/27/2023 7:29 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by Almen123 is split to a separate thread with the subject Is it possible to monitor SLS and SOS functions with drive configuration as above without encoder?. Best regards |
Follow us on