10/29/2023 8:38 AM | |
Joined: 11/30/2021 Last visit: 6/22/2024 Posts: 3 Rating: (0) |
Hello, I am facing problem in browsing the WInCC OS server tags on OPC UA client (OPC Expert) through OPC UA server. I am getting connection of OPC server healthy but when i am trying to import the tags then its showing 0 folder found. (screenshot of OPC expert attached) I have separate OpenPCS7 station and separate Wincc OS servers. I have checked 'Automation Projects' folder where both (SPOSA and downloaded file) the .dcf files are present. Even certificates is also present in PKI folder. I have cheked log file from trace folder which is showing 'GetWinccLicenceinterface failed! (hr=0x80040154) and 'certificates invalid or expired' (Log file attached) Is anybody gone through this type of problem? Any Solution? AttachmentAttachement.zip (212 Downloads) |
Follow us on