11/14/2023 2:01 PM | |
Joined: 2/10/2015 Last visit: 6/26/2024 Posts: 99 Rating:
|
Hello, RFID communication_1 is the right choice for transponder access. Please keep in mind that the TO needs to be updated if changes are made. This is also the case if a different module is selected in a existing TO. You can either create a new TO or downlaod the exisiting one and transfer the start values to the acutal values. |
1/4/2024 11:14 AM | |
Joined: 6/19/2017 Last visit: 6/26/2024 Posts: 8190 Rating:
|
New question published by AutoGen_6930262 is split to a separate thread with the subject Connection with RF166C, RF615R and RF650A via Profibus.. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on