6/9/2009 10:58 AM | |
Joined: 3/3/2008 Last visit: 10/5/2023 Posts: 333 Rating: (51) |
hi can you isolate the I/R module and check the status , may be you could have connected to some other L.T modules which is causing the problem. after isolating check what is the status of led and the drive reay relay as per the S1 dip switch settings. I/R & E/R are same first in english and latter in german --- infeed/regenerative UE & UI are same first in english and latter in german---- uncontrolled infeed Einspeisung : infeed regenerativ : regenerative
Attachmentdrive ready.pdf (723 Downloads) |
Follow us on