1/9/2024 6:40 PM | |
Joined: 5/6/2022 Last visit: 10/11/2024 Posts: 464 Rating: (92) |
Hi Swany, It seems a very strange behavior indeed. From what I understand from your post, this problem only happens to you if you have selected/set something giving it a Pallete color, right? If you select a normal non Pallet color, does it show correctly in the Client? What I would recommend to test is to update the version of WinCC V8 to the latest possible version, in case this behavior has been corrected: "Updates for WinCC V8.0 and WinCC V8.0 ASIA" If not I would create an SR to Siemens Support in case it is some kind of bug or something.... Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
2/2/2024 11:59 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by MustafaQandeel is split to a separate thread with the subject WinCC client shows wrong black color when importing color palettes from the server.. Best regards |
9/25/2024 8:14 PM | |
Joined: 4/16/2017 Last visit: 10/7/2024 Posts: 1 Rating: (0) |
I think this is relevant in WinCC 8.0 update 5 check readme page 41 https://support.industry.siemens.com/cs/ww/en/view/109818723 |
Last edited by: Moderator_Lan at: 09/26/2024 07:08:14link optimized |
|
This contribution was helpful to1 thankful Users |
Follow us on