4/30/2016 5:13 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello If you are operating an Industrial Ethernet CP of the S7-300 as PROFINET IO controller or PROFINET IO device, then you must call the following communication functions in the user program:
Here is a FAQ which explains the usage of these blocks : How do you program communication blocks FC11 and FC12 for the PROFINET IO device? Also Here is a Manual of Std blocks for SIMATIC NET CPs : SIMATIC NET Program blocks for SIMATIC NET S7 CPs - Programming Manual Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |