Industry Online Support
Technical Forum
1/31/2007 4:29 PM | |
Posts: 1 Rating: (0) |
I'm using an ADI4 (or IM174) connected to the 'DP Drive' port on the 317T. I would like to get the diagnostic information from the ADI4, as shown in the attached PDF file. (I.e.. I would like to read the "raw" profibus data - in particular, the Gx_IST2 error codes and any other encoder fault data). Is there a way to do this using the 317T? As possibilities, I'm looking at FB450 'MC_ReadPeriphery', or FB453 'MC_ReadRecord' -- but it doesn't look like these are quite what I want? Any other suggestions for getting Encoder diagnostic information (we are using SSI encoders) would be helpful. Thanks -Craig AttachmentIM174_Manual_Extract.pdf (245 Downloads) |
Follow us on