Industry Online Support
Technical Forum
11/6/2012 1:45 AM | |
Joined: 9/27/2006 Last visit: 5/11/2024 Posts: 12257 Rating: (2666) |
Hello glatocha; The following lik shows the steps to setup a CPU 315-2DP as a Profibus-DP slave to a S5 master: This should be very close to what you are trying to do: How do you operate an S7-300/400 as a DP slave on the PROFIBUS DP when the DP master is an S5 (with IM 308-C)? And this thread might be helpfu, it discusses the same issue you are working onl: DP Slave Problem - Siemens Industry Online Support Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on