7/10/2024 12:30 PM | |
Joined: 12/6/2022 Last visit: 7/11/2024 Posts: 1 Rating:
|
I am currently working on a project where I am using a KTP 900 HMI to communicate with an Emerson PLC (CPE-100) via Modbus TCP/IP protocol. The communication between the HMI and PLC is established and functioning correctly for regular data exchange. However, I am facing challenges in configuring alarms using Modbus addressing. I have created the necessary tags in the HMI and assigned them to the corresponding Modbus addresses, but the alarms are not being triggered as expected. ------------------------------------------------------------------------------------------ |
Last edited by: Wit_Moderator at: 07/11/2024 12:35:28New subject after splitting |
|
Follow us on