7/25/2013 8:05 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (878) |
Hello, 1000 volt - Is it operation voltage or insulation voltage? How much load current capacity & application? |
7/25/2013 8:14 AM | |
Posts: 262 Rating: (45) |
Hello, You can use 3RT1054 for 1000V but maximum current would be 53A. refer the datasheet. Attachment3RT105.pdf (309 Downloads) |
7/25/2013 8:19 AM | |
Joined: 1/6/2011 Last visit: 8/29/2024 Posts: 45 Rating: (0) |
sorry.may i must change the heading. I am looking for 1000V insulation level. Actually I need a replacement for old 3TF series contactor 3TF5044-0XU0whose insulation level is 1000V which can be seen in the catalog. but for 3RT1054 I cannot find the insulation level information. I am attaching the catalog 3TF contactors. In this catalog it is also mentioned that at different operation voltage levels, what is the output KW achieved. So is there a similar catalog for 3RT1054 as well ?AttachmentD:\Manuals\LV\Contactors\3TF AC contactors.pdf (293 Downloads) |
7/25/2013 8:34 AM | |
Joined: 1/6/2011 Last visit: 8/29/2024 Posts: 45 Rating: (0) |
thanx a lot valli. |
7/25/2013 8:51 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (878) |
Yes, please see the attachment.
Attachment3RT105 data sheet.zip (292 Downloads) |
Follow us on