9/1/2022 3:02 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
What about PLC logic? Have you loaded it & configured interface signals? |
9/1/2022 12:29 PM | |
Joined: 10/19/2016 Last visit: 5/20/2024 Posts: 286 Rating: (0) |
I don't use the STARTER, i configure the drive manually. Attached the S7 archive and NC-drive data archive. Usually the recognition is automatic, it always worked in this way Edit: I don't know if this is the problem, but I put 20050 and 20060 to "0" (all tabs) to avoid errors related to cartesian axis AttachmentMHSS37 6000.zip (186 Downloads) |
Last edited by: gtsolid at: 09/01/2022 12:29:57Last edited by: gtsolid at: 09/01/2022 13:04:39Last edited by: gtsolid at: 09/02/2022 06:45:55Last edited by: gtsolid at: 09/02/2022 09:14:21𓋹 |
|
9/4/2022 5:03 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Hello, No logical drive addresses found in your NC as well as in PLC also Sinamics interface is not established nor found any drive. Project is incomplete, i.e. not commissioned properly. I suggest you to refer SINUMERIK 840D sl Commissioning CNC: NC, PLC, Drive manual. |
This contribution was helpful to1 thankful Users |
Follow us on