1/7/2020 10:26 AM | |
Joined: 10/26/2011 Last visit: 8/30/2024 Posts: 762 Rating: (191)
|
If your monitor have 4 inputs for 4 PCs, than it is possible to use one monitor.
|
SIMATIC PCS 7 - Overview |
|
1/8/2020 8:17 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello Glads, with the Advanced Process Graphic (APG) you can display up to four different process pictures from one OS client on a single screen as quadrants. The process pictures are displayed in four frames that have half the width and height of the available screen. A quadrant button allows fast transfer and change of process pictures. With regards |
Follow us on