7/26/2017 11:59 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi, with ethernet-cable. then you need to project the I-device function. See this FAQ/application sample: Configuration and application of PROFINET I-Device function Note: connection to the TP900 is not Profinet. You need to establish a HMI-connection over ethernet. hope this helps, regards, |
FCK WAR! |
|
7/26/2017 12:07 PM | |
Joined: 4/30/2013 Last visit: 2/6/2023 Posts: 103 Rating: (4) |
HI. Infact I am looking for a 5 port swicth eg.CSM 1277 module or something like this. |
Rate it if it is helphul. |
|
7/26/2017 12:14 PM | |
Joined: 4/30/2013 Last visit: 2/6/2023 Posts: 103 Rating: (4) |
HI. What the difference between profinet and ethernet?
|
Rate it if it is helphul. |
|
7/26/2017 2:56 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi, Profinet is a protocoll that runs on Industrial Ethernet. It is for I/O-communication between IO-controller and IO-devices. Maybe this manual is intresting for you: SIMATIC PROFINET System Description hope this helps, regards, |
FCK WAR! |
|
Follow us on