3/3/2021 9:24 AM | |
Joined: 4/9/2018 Last visit: 8/31/2022 Posts: 16 Rating:
|
Hi guys. System: PCS7 v8.0 SP2 CPU: 410-5H single , FW 8.1.0 Any ideas what happend here? see attached diagnostics export, trouble starts at event 289. There is a total of 7cpus in the project, three of these are 410-5H and the rest 416, all of the 410 cpus have had this problem atleast once. The cpu goes in to Defective mode and triggers a complete memory reset. The powersupply is healthy. System is legacy so siemens is not very helpful, guess we got to upgrade.. AttachmentDiagnose.txt (554 Downloads) |
L P#Problem |
|
12/30/2021 2:25 PM | |
Joined: 12/30/2016 Last visit: 6/7/2024 Posts: 1 Rating:
|
U need update firmware for your cpu's. Version 8.2.1 and further hasn't problem defective!!! |
Follow us on