3/12/2010 10:28 PM | |
Joined: 9/19/2009 Last visit: 7/5/2024 Posts: 459 Rating: (84) |
Hello Everybody. I have an old PC Simatic 670 with ProTool Runtime. So I want to transfer my project to 670, but I don´t know how I can´t do it. What port I need to use it? I have a serial port RS232, and I have a CP5611 Rs-485 MPI/DP. When I power on the panel, what is the first I need do it. In others TP/OP I don´t have any doubt ,because the first screens is for transfer it! but with this panel, I don´t know how I need to procedure. Thanks advanced |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
3/16/2010 4:40 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1166)
|
Dear JM76, Perhaps this link might help: Transferring the Protool/Pro runtime file (*.fwd) from the configuration computer to the visualization PC with the Protool/Pro RT loader Best regards, Wizard |
3/17/2010 11:25 AM | |
Joined: 9/19/2009 Last visit: 7/5/2024 Posts: 459 Rating: (84) |
Ok! Thank you Mr Wizard, I have not saw this link before! |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on