Industry Online Support
Technical Forum
5/30/2010 9:01 PM | |
Joined: 3/21/2006 Last visit: 2/10/2025 Posts: 10239 Rating:
|
Hello, Seems you have problem in Profibus network (DP2 "row"). And in your program don't have Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails? Back to your question. Look at What is the difference between the PC Adapter and the TS Adapter in communication between the PC and the S7? how to use TC Adapter. best regards, Hristo Mihalev |
Follow us on