6/25/2010 3:13 PM | |
Joined: 9/28/2005 Last visit: 8/27/2024 Posts: 2957 Rating: (242)
|
Hi, UMENCHO Never forget this link http://support.automation.siemens.com/WW/view/en/28979404 |
Best regards, |
|
6/25/2010 3:16 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Hi Darius, What about this links? |
6/25/2010 3:19 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Exactly, you are right. And also Eric know this. Just he has other ideas... |
6/28/2010 7:28 AM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Hello Eric, Yes, but SP3 is "freeware". You need to have only internet access. Also is possible to download in your home. Believe me this is the only way. Best regards, Hristo Mihalev |
6/28/2010 7:42 AM | |
Joined: 5/28/2008 Last visit: 10/12/2024 Posts: 4515 Rating: (839) |
Please think again before migration to Windows 7. You have to check the comptability of all SIMATIC software you are using with Windows 7. You will be able to use WinCC flex. 2008 SP2. Please check these useful links. Are STEP 7 and its optional software products compatible with Windows 7? Which SIMATIC software packages are compatible with which Microsoft Windows operating system and with STEP 7 V5.4? Which version of STEP 7 is compatible with which version of Internet Explorer? Tips and tricks to check STEP 7- compatibility Hope this helps. |
Ayman Elotaify |
|
6/29/2010 7:29 AM | |
Posts: 487 Rating: (36) |
HI Let me explain the problem , our IT service does not work under a democratic system but rather a dictator type set-up.We only have 'limited' rights on our computers and installing SP3 is not one of them but we are twisting their arms and legs and suddenly they work in a burocratic system meaning that after filling in about 200 forms they will consider our request ... should only take about a month or so !!! So for the moment we will have to use our field PG for all the development work. But thanks for all the answers. Bye Eric |
This contribution was helpful to1 thankful Users |
Follow us on