Industry Online Support
Technical Forum
9/14/2022 5:31 AM | |
Joined: 4/9/2016 Last visit: 10/21/2022 Posts: 13 Rating:
|
Hello I made a program that switches between five outputs with one push button. In fact, the program is supposed to switch between 5 different counters. In the simulation, it works fine, but via the controller, the outputs light up randomly. I'm sure this way is not correct, but I have no idea how to do it in a different way. AttachmentCOUNTERS 5.zip (67 Downloads) |
9/14/2022 6:02 AM | |
Joined: 12/18/2014 Last visit: 1/30/2023 Posts: 29058 Rating:
|
See attachment, try this.
AttachmentCOUNTERS 5_V2.zip (91 Downloads) |
Follow us on