6/1/2010 10:42 AM | |
Posts: 39 Rating:
|
Hello, Ben starting OP25 there is a error " 613 DB error No:101 (0,42) " . Is this mean that the dw memory between DW0 and DW42 is not exist ? Thank you. |
6/1/2010 10:59 AM | |
Joined: 4/24/2006 Last visit: 3/21/2025 Posts: 8904 Rating:
|
Dear obyone_2, Here is link to manual: Operator panel OP25, OP35, OP45 See appendix D Here is explanation: 613 The specified data block with DB no. (starting DW and end DW) does not exist in the controller or is too short. (Values in parentheses: First data word, last data word) |
6/1/2010 3:42 PM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
Hello, M27C1001-12F1 this is 1 MBIT (128KB X8) UV EPROM AND OTP ROM (more at datasheet) To take backup from OP25 is possible only with Memory Card. Take a look at perator Panel OP25, OP35, OP45 how is possible to make backup restore. And if you don't have Jeida/PCMCIA module I think is not possible. Best regards, Hristo Mihalev |
6/1/2010 4:09 PM | |
Posts: 39 Rating:
|
I haven't got PCMCIA/JEIDA :( is there any solution ? |
6/1/2010 4:56 PM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
There isn`t any solution without a card. |
Follow us on