2/11/2015 4:49 PM | |
Joined: 6/24/2013 Last visit: 6/1/2024 Posts: 1608 Rating: (415) |
Hi All
To do any operation user defined functions and data type must be used. I have created library which supports Long Real stored as Array[1..2] of DWORD. Lbrary contains: - Conversion Functions (LReal<->Real, LReal<->DInt) - Comparators (Equal, Not Equal, Less Than, Less Equal, Greater Than, Greater Equal) - Maths (Add, Sub, Mul, Div, Neg (*-1), Abs) - PAC3200 Energy Meter conversion Function which converts LReal to DInt in kWh and Int in Wh which are convenient to display on HMI/SCADA Attached to this post AttachmentIS0034_LONGREAL.zip (999 Downloads) |
Last edited by: Piotr.M at: 9/7/2015 10:05:33 AMLast edited by: Piotr.M at: 9/7/2015 10:06:07 AMLast edited by: Piotr.M at: 9/7/2015 2:50:20 PMLast edited by: Piotr.M at: 9/8/2015 11:31:04 AM |
|
This contribution was helpful to5 thankful Users |
9/30/2019 12:28 PM | |
Joined: 6/24/2013 Last visit: 6/1/2024 Posts: 1608 Rating: (415)
|
Hi Library converted to TIA v15 attached Regards Piotr AttachmentIS0034_LONGREAL_TIA.zip (368 Downloads) |
This contribution was helpful to3 thankful Users |
Follow us on