9/1/2008 9:27 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hi, normaly the GSD Data shouldinstall. What STEP 7 Version did you use? I use V5.4 SP3 and i could select the GSD file for the TP177B (see attachment). Furthermore. In the attachment you will find the gsd file for the TP which you can install AttachmentSiem8107.zip (2025 Downloads) |
This contribution was helpful to
2 thankful Users |
9/1/2008 9:38 AM | |
Joined: 4/24/2006 Last visit: 4/25/2025 Posts: 8969 Rating:
|
Hi gezgin1500, They already told you where to find GSD-file. See also this link: http://support.automation.siemens.com/WW/view/en/29339779 But why do you need GSD-file? It's only necessary when you want to use DP-direct keys or when you want to connect to S5-master. When you want to connect to S7-master, you' ll have to set communication channel right. When WinCC flexible is integrated in Step 7, you can see Panel in NETPRO. (not in hardware configuration) Best regards, Wizard |
This contribution was helpful to
2 thankful Users |
1/18/2020 3:11 PM | |
Posts: 3 Rating:
|
DEAR, CAN ANYONE HELP FIND GSD FILE HMI MODEL: TP177B PN/DP-6CSTN SERIES: 6AV6642-0BA01-1AX1 REGARDS HUSSAIN |
1/19/2020 3:02 AM | |
Posts: 3 Rating:
|
ITS NOT SUTABLE FOR TP177B |
1/20/2020 11:30 AM | |
Joined: 8/3/2017 Last visit: 6/11/2024 Posts: 1086 Rating:
|
Hi, well.. I have a look on the link and there is following written:
Did you installed WinCC flexible or ProTool? |
Please, check out the forum search to find already existing topics regarding your issue and to get some hints. |
|
Follow us on