10/1/2023 10:40 AM | |
Joined: 9/9/2023 Last visit: 7/18/2024 Posts: 24 Rating: (0) |
The 300c° was measured without a fan.If the fan maintains the stove temperature at 120°C this does not pose a problem. |
10/1/2023 11:09 AM | |
Joined: 12/18/2014 Last visit: 11/18/2024 Posts: 34239 Rating: (4263)
|
If I understand it correctly, 25% is the minimum desired performance. By the way: https://www.niko.eu/-/downloadfile/eaa353bcd66948b587daae5d00ac64d2 |
10/1/2023 11:23 AM | |
Joined: 12/18/2014 Last visit: 11/18/2024 Posts: 34239 Rating: (4263)
|
All I can say is that the Niko dimmer module is not suitable for inductive loads (e.g. fans). |
Follow us on