Industry Online Support
Technical Forum
1/7/2011 2:59 PM | |
Posts: 1 Rating:
|
What is the allowable coil voltage range? |
1/8/2011 10:17 PM | |
Posts: 2930 Rating:
|
Hi, LOGO!Contact is available for 230V AC and 24V DC. Have look to the LOGO! manual for more information. Hope this helps |
1/10/2011 11:14 AM | |
Posts: 173 Rating:
|
The LOGO! Contact 24 or 230V coil versions are based on the Siemens Contact 3TG10. The information about this is available from the LOGO! website www.siemens.com/logo http://www.automation.siemens.com/mcms/industrial-automation-systems-simatic/en/manual-overview/tech-doc-controllers/Pages/Default.aspx#LOGO! From the menu on the left side, the LOGO! Contact is mentioned. Then go to "Overview of Topics" on the right side, there is a link to Technical Documentation LOGO! At the bottom of the grey LOGO! block, is the link to the Contact information. The direct link from the Support Site is http://support.automation.siemens.com/WW/view/en/6006460 Hope this helps! |
Follow us on