3/31/2015 2:50 PM | |
Joined: 9/27/2006 Last visit: 9/22/2024 Posts: 12282 Rating: (2684) |
Hello JC; This update popped up when searching for information on your module (in the forum Search function, see the attached file):
Support Packages for the hardware catalog in the TIA Portal (HSP) See if it can help you out. hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
3/31/2015 3:15 PM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011) |
Hello,
the MLFB Number 6ES7155-6AA00-0BN0 doesn't mean the Inferfacemodule ! To configure this in TIA you must choose the Module with the Ordernumber 6ES7155-6AU00-0BN0.
|
Last edited by: ChristophD at: 3/31/2015 3:18:50 PM |
|
This contribution was helpful to18 thankful Users |
4/18/2016 5:15 PM | |
Joined: 8/30/2010 Last visit: 8/31/2024 Posts: 31 Rating: (1) |
Dear, I am not getting 6es7155 -6AA00 - 0BN0 I have checked in complete HSP downloaded ZIP folder Thanks |
4/18/2016 8:11 PM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hello, read he post from 2015 and you will find the answer to your problem .
Christoph |
4/18/2016 8:39 PM | |
Joined: 5/28/2008 Last visit: 9/21/2024 Posts: 4515 Rating: (839) |
Hello, Please follow ChristophD answer. You will never get the partnumber 6ES7 155-6AA-0BN0 in the catalog as it's consists of IM + 2 RJ sockets Please search only for part number "6ES7 155-6AU00-0BN0" Please have a look here: SIMATIC ET 200SP - Interface Modules and BusAdapters |
Ayman Elotaify |
|
5/24/2016 4:22 PM | |
Joined: 8/21/2008 Last visit: 8/23/2024 Posts: 141 Rating: (6) |
I have TIA V13 Update 8. I downloaded the supporting package mentioned in the earlier thread. Even after doing this, hardware 6ES7 155-6AU00-0BN0 is not seen under the section ST200SP for TIA V13. In S7, I am able to find it. What should I do? rgds, Rakesh |
Last edited by: RBM at: 5/24/2016 4:22:58 PMLast edited by: RBM at: 5/24/2016 4:28:49 PM |
|
5/24/2016 4:31 PM | |
Joined: 8/21/2008 Last visit: 8/23/2024 Posts: 141 Rating: (6) |
Added picture of support package system showing 6ES7155-6AU00-0xN0 is installed |
5/25/2016 1:25 AM | |
Posts: 1529 Rating: (202) |
Because it is distributed I/O and not a controller. Add it using Devices and Networks. |
This contribution was helpful to4 thankful Users |
11/26/2021 9:29 AM | |
Joined: 10/19/2014 Last visit: 9/19/2024 Posts: 3 Rating: (0) |
I want to use 6ES7-155-6AA01-0BNO in Tia portal v13 Sp2 I update support pakage and also gsd file But cataloge hardware not update it Only 6ES7-155-6AU00-0BN0 is in there How can solve it ? |
Follow us on