Industry Online Support
Technical Forum
11/23/2010 7:36 AM | |
Posts: 3 Rating:
|
Hello, I have a problem with two 6RA24 DC drivescoupled to gearbox on rubber mixer application. Both drives are in Master and Slave configuration driven true Profibus and S5.One of the drive stops with no reason andno fault message on the display. Usually Master drive stops but I have seen also Slave drive stopped. Slave drive parameter P880 for all four words is144. I don’t know what it means and I don’t have any manuals with F144 description. In Master drive P880 value is 3, 4, 4, 4.Can you please give me any advice on this issue? Thanks in advance, Janez Attachmentmaster_slave.zip (186 Downloads) |
11/23/2010 9:00 AM | |
Posts: 3 Rating:
|
Thanks for replay, where can I get manuals for technological card SYMADIN D PT10P1? |
11/23/2010 10:32 AM | |
Posts: 3 Rating:
|
O.K. Than you. |
Follow us on