Industry Online Support
Technical Forum
5/14/2010 5:03 AM | |
Joined: 8/25/2006 Last visit: 7/15/2024 Posts: 2207 Rating:
|
Look herefor one example. Also I think (but I'm not sure) you can connect to drives via Profibus without IE/PB Link (as in example) when using Drive-ES. |
5/14/2010 5:46 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Hello, Yes, KSN is right. You could access to all drives (which are connected in profibus line) using Drive ES software. Let's assume you have access to the S7 CPU via ethernet from control room. (in rolling mill this is common way). So, putting this PC in Netpro configuration plus necessaries settings you will have access to monitor all drives via DriveMon. Look at http://support.automation.siemens.com/WW/view/en/22794082 Best regards, Hristo Mihalev |
5/14/2010 12:44 PM | |
Posts: 27 Rating:
|
Dear Xiaotang Yes you can access all the drives on the profibus network using Drive ES in the Eng. PC RegardsBist |
Follow us on