7/28/2014 5:30 AM | |
Joined: 8/25/2006 Last visit: 9/5/2024 Posts: 2208 Rating: (278) |
Hello. Look in themanual, chapter 9.18. 1.You could try to use B0129 in P580 from Status word 1 (look at function diagram G182). For this set P594=K0010 (look at G188 and G113). As speed setpoint use abs. value of AI 4,5, set P703=1 and use K0011. 2. For 1Q drive it is only possible to reverse direction of rotation or braking using field reversal. Ramp-down time will not work while you decrease setpoint.
|
10/13/2014 12:59 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
7/5/2017 2:12 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (171) |
New question published by RoxTech is split to a separate thread with the subject SIMOREG DC master with T400 technological card. Best regards |
Follow us on