Industry Online Support
Technical Forum
4/16/2012 7:01 AM | |
Joined: 3/30/2010 Last visit: 7/26/2021 Posts: 13 Rating:
|
Hello, Here I have problem to open the S7200 PLC backup which i got from customer. As per customer said,this program open in his system. he created program in V4.0.3.08 and i have V4.0.7.10 & V4.0.8.06 system higher than created one. when i tried to open the backup i can't view anything also error come. ( All or part of th e path is invalid) please check this program in your system and give me the feedback. See the attached program Kiran Sonar. Attachment项目0907版.zip (350 Downloads) |
4/16/2012 7:20 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating:
|
Hello, All you have to do is rename the MWP- file and it will open. Regards, Marcjan Attachmentmarcjan.zip (416 Downloads) |
Problem solved? |
|
This contribution was helpful to
1 thankful Users |
Follow us on